1.35.18.14 TWIHSx_CallbackRegister Function
C
/* x = TWIHS instance number */ /* TWIHS master mode */ void TWIHSx_CallbackRegister(TWIHS_CALLBACK callback, uintptr_t context) /* TWIHS slave with interrupt enabled */ void TWIHSx_CallbackRegister(TWIHS_SLAVE_CALLBACK callback, uintptr_t context)
Summary
Sets the pointer to the function (and it's context) to be called when the given TWIHS transfer events occur.
Description
This function sets the pointer to a client/application function to be called "back" when the given TWIHS transfer events occur. It also passes a context value (usually a pointer to a context structure) that is passed into the function when it is called. The specified callback function will be called from the peripheral interrupt context.
Precondition
TWIHSx_Initialize must have been called for the associated TWIHS instance.
Parameters
Param | Description |
---|---|
callback | A pointer to a function with a calling signature defined by the TWIHS_CALLBACK (in TWIHS master mode) or TWIHS_SLAVE_CALLBACK (in TWIHS slave mode) data type. Setting this to NULL disables the callback feature. |
context | A value (usually a pointer) which is passed (unused) into the function identified by the callback parameter |
Returns
None.
Example
TWIHS master mode
void TWIHS1_Callback(uintptr_t context) { if(TWIHS1_ErrorGet() == TWIHS_ERROR_NONE) { //Transfer is completed successfully } else { //Error occurred during transfer. } } // Register Callback function which is defined above TWIHS1_CallbackRegister(TWIHS1_Callback, (uintptr_t)0);
TWIHS slave in non-blocking/interrupt mode
bool TWIHS1_Callback ( TWIHS_SLAVE_TRANSFER_EVENT event, uintptr_t context ) { uint8_t rxData; uint8_t txData; switch(event) { case TWIHS_SLAVE_TRANSFER_EVENT_ADDR_MATCH: // Handle address match event break; case TWIHS_SLAVE_TRANSFER_EVENT_RX_READY: // TWIHS master is writing data to TWIHS slave. // Read the received data byte. rxData = TWIHS1_ReadByte(); break; case TWIHS_SLAVE_TRANSFER_EVENT_TX_READY: // TWIHS master is reading data from TWIHS slave. // Provide data to TWIHS master. TWIHS1_WriteByte(txData); break; } } // Register Callback function which is defined above TWIHS1_CallbackRegister(TWIHS1_Callback, (uintptr_t)0);
Remarks
When TWIHS is configured in master mode, the callback function prototype is TWIHS_CALLBACK.
When TWIHS is configured in slave mode, the callback function prototype is TWIHS_SLAVE_CALLBACK.