1.25.9.5 OTPC_LockPacket Function
C
otpc_error_code_t OTPC_LockPacket(uint16_t headerAddress);
Summary
Locks the packet
Description
Lock a packet with given address. No further modification are permitted.
Precondition
OTPC_Initialize() function must have been called first and a valid packet should exist at the address.
Parameters
Param | Description |
---|---|
headerAddress | Address of the packet |
Returns
OTPC error code
Example
OTPC_Initialize(); OTPC_LockPacket(headerAddress);
Remarks
None