1.42.5.2 HEMC_DisableECC Function

C

bool HEMC_DisableECC( uint8_t chipSelect )

Summary

Disable the ECC for the given chip select.

Description

This function disable the ECC for the given chip select of the HEMC peripheral.

Precondition

None.

Parameters

Param Description
chipSelect The chip select for which ECC is disabled.

Returns

True if ECC was disable for this chip select, False otherwise.

Example

HEMC_DisableECC(0);

Remarks

None.