1.7.14.12 GPIO_PinWrite Function

C

void GPIO_PinWrite(GPIO_PIN pin, bool value)

Summary

Writes the logic level of the selected pin.

Description

This function writes/drives the "value" on the selected I/O line/pin.

Precondition

The desired pin must be configured as an output pin.

Parameters

Param Description
pin One of the IO pins from the enum GPIO_PIN
value value to be written on the selected pin:
- true set pin to high (1).
- false clear pin to low (0).

Returns

None.

Example

GPIO_PinWrite(GPIO_PIN_RB3, true);

Remarks

None.