1.12.6.8 CORETIMER_PeriodSet Function
C
void CORETIMER_PeriodSet(uint32_t period);
Summary
Sets the period value of a Core timer.
Description
This function writes the period value. When timer counter matches period value counter is reset and interrupt can be generated.
Precondition
CORETIMER_Initialize() function must have been called first.
Parameters
Param | Description |
---|---|
period | new period value to set for timer |
Returns
None.
Example
uint32_t period = 0x100;
CORETIMER_Initialize();
CORETIMER_PeriodSet(period);
Remarks
Should be generated for periodic interrupt mode only.