1.34.11.6 PWMx_ChannelDutySet Function
C
/* x = PWM instance number */ void PWMx_ChannelDutySet(PWM_CHANNEL_NUM channel, uint32_t duty); void PWMx_ChannelDutySet(PWM_CHANNEL_NUM channel, uint16_t duty);
Summary
Writes the duty cycle value of given PWM channel
Description
This function writes the duty cycle value in double buffer register. Update to the actual duty cycle register happens at the next period border.
Precondition
PWMx_Initialize() function must have been called first for the associated instance. And associated channel must be running.
Parameters
Param | Description |
---|---|
channel | PWM channel number |
duty | duty cycle value which determines ON time of waveform. Refer the generated header for the exact data type |
Returns
channel - PWM channel number
duty - duty cycle value
Example
PWM0_Initialize(); PWM0_ChannelsStart(PWM_CHANNEL_0_MASK); PWM0_ChannelDutySet(PWM_CHANNEL_0, 0x200);
Remarks
Refer the generated header file for the exact function signature