1.19.20.7 TMR1_PeriodGet Function
C
uint16_t TMR1_PeriodGet(void);
Summary
Reads the period value of given timer.
Description
This function reads the value of period of given timer.
Precondition
TMR1_Initialize() function must have been called first.
Parameters
None.
Returns
period - The timer's period value.
Example
uint16_t period; TMR1_Initialize(); period = TMR1_PeriodGet();
Remarks
None.