1.35.16.26 TCx_CHy_CaptureStatusGet Function
C
/* x = TC instance number, y = channel number */ TCx_CAPTURE_STATUS TCx_CHy_CaptureStatusGet ( void )
Summary
Identifies status of the capture events
Description
This function returns the status of the events that occur in capture mode.
Precondition
TCx_CHy_TimerInitialize() function must have been called first for the given channel to configure channel in capture mode.
Parameters
None
Returns
TCx_CAPTURE_STATUS - status of the capture events
Example
uint16_t capture; if ((TC0_CH1_CaptureStatusGet() & TC_CAPTURE_A_LOAD) == true) { capture = TC0_CH1_CaptureAGet(); }
Remarks
This function is applicable only for capture mode. Event status bits are cleared after reading the status register.