3.26.19 Static Memory Controller (SMC)

The Static Memory Controller (SMC) generates the signals that control the access to the external memory devices or peripheral devices. It has 6 Chip Selects and a 26-bit address bus. The 32-bit data bus can be configured to interface with 8-, 16-, or 32-bit external devices. Separate read and write control signals allow for direct memory and peripheral interfacing. Read and write signal waveforms are fully parametrizable.

The SMC can manage wait requests from external devices to extend the current access. The SMC is provided with an automatic slow clock mode. In slow clock mode, it switches from user-programmed waveforms to slow-rate specific waveforms on read and write signals. The SMC supports asynchronous burst read in page mode access for page size up to 32 bytes.

Using The Library

Static Memory Controller (SMC) is initialized as configured in the MCC as part of System Initialization.

Library Interface

Static Memory Controller peripheral library provides the following interfaces:

Functions

NameDescription
SMC_InitializeInitializes Static Memory Controller (SMC) interface
SMC_DataAddressGetReturns the External Bus Interface (EBI) address for the requested chip select number
SMC_CommandWriteWrites command to the External Bus Interface (EBI) address
SMC_CommandWrite16Writes 16-bit command to the External Bus Interface (EBI) address
SMC_AddressWriteWrites address to the External Bus Interface (EBI) address
SMC_AddressWrite16Writes 16-bit address to the External Bus Interface (EBI) address
SMC_DataWriteWrites data to the External Bus Interface (EBI) address
SMC_DataWrite16Writes 16-bit data to the External Bus Interface (EBI) address
SMC_DataReadReads data from the External Bus Interface (EBI) address
SMC_DataRead16Reads 16-bit data from the External Bus Interface (EBI) address
SMC_CallbackRegisterSets the pointer to the function (and it's context) to be called when the given SMC's interrupt occurred
PMECC_CallbackRegisterSets the pointer to the function (and it's context) to be called when the given PMECC's interrupt occurred
PMERRLOC_CallbackRegisterSets the pointer to the function (and it's context) to be called when the given PMERRLOC's interrupt occurred
PMECC_DataPhaseStartEnables PMECC Write access and start data phase
PMECC_StatusIsBusyReturns PMECC busy status
PMECC_ErrorGetReturns PMECC error
PMECC_RemainderGetReturns PMECC remainder
PMECC_ECCGetReturns error correction code (ECC)
PMERRLOC_ErrorLocationGetFind and returns error location of memory
PMERRLOC_ErrorLocationDisableDisables error location of memory
PMERRLOC_SigmaSetSet sigma value to the PMERRLOC register
PMERRLOC_ErrorLocationFindNumOfRootsFind the number of roots using PMERRLOC acceleration

Data types and constants

NameTypeDescription
SMC_CALLBACKTypedefDefines the data type and function signature for the SMC peripheral callback function
PMECC_CALLBACKTypedefDefines the data type and function signature for the PMECC peripheral callback function
PMERRLOC_CALLBACKTypedefDefines the data type and function signature for the PMERRLOC peripheral callback function