3.1.10 RTOS Timer
The RTOS Timer is a low-power, 32-bit timer designed to operate on the 32kHz oscillator which is always available during all chip sleep states. This allows firmware the option to sleep the processor and wake after a programmed amount of time. The timer may be used as a one-shot timer or a continuous timer. When the timer transitions to 0 it is capable of generating a wake-capable interrupt to the embedded controller. This timer may be halted during debug by hardware or via a software control bit
Using the Library
The below example generates periodic timeout using the RTOS peripheral. A callback is
registered with the RTOS timer and an LED is toggled in the callback
function.
void rtos_tmr_callback(uintptr_t context)
{
LED0_Toggle();
}
int main ( void )
{
/* Initialize all modules */
SYS_Initialize ( NULL );
RTOSTimer_CallbackRegister(rtos_tmr_callback, 0);
RTOSTimer_Start();
while ( true )
{
/* Maintain state machines of all polled MPLAB Harmony modules. */
SYS_Tasks ( );
}
/* Execution should not come here during normal operation */
return ( EXIT_FAILURE );
}
Library Interface
Functions
Name | Description |
---|---|
RTOSTimer_Initialize | Initializes given instance of RTOS timer peripheral. |
RTOSTimer_PeriodGet | Returns the period value for the RTOS timer |
RTOSTimer_PeriodSet | Sets the time period for the RTOS timer |
RTOSTimer_Resume | Resumes the RTOS timer |
RTOSTimer_Start | Starts the RTOS timer |
RTOSTimer_Stop | Stops the RTOS timer |
RTOSTimer_Halt | Halts the RTOS timer |
RTOSTimer_FrequencyGet | Returns the input frequency of the RTOS timer |
RTOSTimer_CounterGet | Returns the timer counter value for the RTOS timer |
RTOSTimer_CallbackRegister | Allows application to register a callback with the PLIB |
Data types and constants
Name | Type | Description |
---|---|---|
RTOS_TMR_CALLBACK | Typedef | Defines the data type and function signature for the RTOS timer peripheral callback function. |