3.9.3 Stack Pointer Overflow
There is a Stack Limit register (SPLIM) associated with the Stack Pointer
that is reset to 0x00000000. SPLIM is a 32-bit register, but SPLIM[1:0] is fixed to
‘00’, because all stack operations must be long word-aligned. To match
the Stack Pointer, the device address space is limited to 24-bits, so the upper 8-bits of
SPLIM are always all 0.
The stack overflow check will not be enabled until a word write to SPLIM occurs, after which time it can only be disabled by a device reset. All Effective Addresses generated using W15 as a source or destination are compared against the value in SPLIM. Should the Effective Address be greater than the contents of SPLIM, then a stack error trap is generated.
If stack overflow checking has been enabled, a stack error trap will also occur if the W15 Effective Address calculation wraps over the end of data space (0x00FFFFFF).