5.1 Configuring Time Aware Shaper using Web GUI
To configure the Time Aware Shaper, perform the following steps:
- To configure PTP 802.1AS, see Configuring a PTP Clock Instance using Web GUI.
- Click VLANs > Configuration, the Global VLAN Configuration page opens. In the Mode list, click Hybrid for both the ingress and the egress ports (see the following figure).
Figure 5-2. Global VLAN Configuration - Click Save.
- Click QOS > Port Classification. The QoS Port Classification page opens.
- To enable the port, find the required port under
the Tag Class column and click
Disabled; this will switch it to
Enabled (see the following figure).
Figure 5-3. QoS Port Classification - Enable Tag Classification on the Egress port.
Figure 5-4. QoS Ingress Port Tag Classification 
- Click Save.
- Click TSN > TAS > Ports. The TAS Configuration Parameters page opens.
Figure 5-5. TAS Configuration Parameters - To set the GCL Length, type a suitable number in the GCL Length text box.
- To set the cycle time, type appropriate values in the Value, Unit, and Extension, ns text boxes.
- Click Save.
- Under GCL, click Configure. The GCL Configuration page opens.
Figure 5-6. GCL Configuration 
- To set the gate state and time interval, select the appropriate check boxes and type a suitable value in the nanoseconds text box (see the following figure).
- Click Save.
- Click Back, the TAS Configuration Parameters page opens.
Figure 5-7. TAS Configuration Parameters - To enable TAS, select the Enabled check box.
- To perform config change, select the Config Change check box.
- Click Save.