1.5 Configuring a PTP Boundary Clock using Web GUI
To configure a boundary clock, perform the following steps:
- Click Configuration > PTP.
- Click Add New PTP Clock.
- Configure the following properties:
- HW Domain = 0
- Device Type = Ord-Bound
- Profile = 1588
Figure 1-11. Create Boundary Clock Instance 
- Click Save.
- Click the Clock Instance link.
- The PTP Clock’s Configuration and Status page opens. Configure the following properties:
- Under the Port Enable and Configuration area, select the suitable ports.
- Under the Clock Default Dataset area, set the following:
- From the 2 Step Flag drop-down list, select True.
- In the Pri1 text box, type a lower number than the PTP slave.
- Under Port Enable and Configuration area, click Ports Configuration. The PTP clock’s Port Data Set Configuration page opens.
Figure 1-12. Configure Boundary Clock Instance - Click the required dom mode, p2p or e2e.
- Click Save.