10.2.5 Data Memory Allocation Macros
The sys/attribs.h header file provides many macros for commonly
used attributes in order to enhance code readability.
__section__(s) |
Apply the section attribute with section name
s. |
__unique_section__ |
Apply the unique_section attribute. |
__ramfunc__ |
Locate the attributed function in the RAM function code section. |
__longramfunc__ |
Locate the attributed function in the RAM function code section and apply
the longcall attribute. |
__longcall__ |
Apply the longcall attribute. |
__ISR(v,ipl) |
Apply the interrupt attribute with priority level
ipl and the vector attribute with vector
number v. |
__ISR_AT_VECTOR(v,ipl) |
Apply the interrupt attribute with priority level
ipl and the at_vector attribute with
vector number v. This macro is especially useful on PIC32
devices that feature variable vector offsets. |
__ISR_SINGLE__ |
Specifies a function as an Interrupt Service Routine in single-vector mode. This places a jump at the single-vector location to the interrupt handler. |
__ISR_SINGLE_AT_VECTOR__ |
Places the entire single-vector interrupt handler at the vector 0 location. When used, ensure that the vector spacing is set to accommodate the size of the handler. |