10.2.1 Non-Auto Variable Allocation
Non-auto variables (those with permanent storage duration)
are located by the compiler into any of the available data banks. This is done in a
two-stage process: placing each variable into an appropriate section and later linking
that section into data memory.
The compiler considers three categories of non-auto variable
which all relate to the value the variable should contain by the time the program
begins. The following sections are used for the categories described.
.pbss- These sections are used to store variables which use thepersistentattribute, whose values should not be altered by the runtime start-up code. They are not cleared or otherwise modified at start-up..bss- These sections (also.sbss) contain any uninitialized variables, which are not assigned a value when they are defined, or variables which should be cleared by the runtime start-up code..data- These sections (also.sdata) contain the RAM image of any initialized variables, which are assigned a non-zero initial value when they are defined and which must have a value copied to them by the runtime start-up code.
Note that the data section used to hold initialized variables is the section that holds
the RAM variables themselves. There is a corresponding section (called
.dinit) that is placed into program memory (so it is non-volatile)
and which is used to hold the initial values that are copied to the RAM variables by the
runtime start-up code.