31.6.4 mips_iir16_setup
Description
Rearranges the coefficients from the input array, bq, into the output array coeffs, which is used by the mips_iir16() function. The number of biquad sections to process is given by the parameter B.
Include
dsplib_dsp.h
Prototype
void
mips_iir16_setup
(
int16 *coeffs,
biquad16 *bq,
int B
);
Argument
coeffs: Output array holding 4B coefficients rearranged for mips_iir16().
bq: Input array holding Q15 coefficients for B biquad sections.
B: Number of biquad sections.
Return Value
None.
Remarks
None.
Notes
This function is implemented in C.