20.2 Using Inline Assembly Language
Within a C/C++ function, the asm statement may be used to
insert a line of assembly-language code into the assembly language that the compiler
generates. Inline -assembly has two forms: simple and extended.
In the simple form, the assembler instruction is written using the syntax:
asm ("instruction");
where instruction is a valid assembly-language construct. If you are
writing inline assembly in ANSI C programs, write
_ _asm_ _ instead of
asm.
In an extended assembler instruction using asm, the operands of
the instruction are specified using C/C++ expressions. The extended syntax is:
asm("template" [ : [ "constraint"(output-operand) [ , ... ] ]
[ : [ "constraint"(input-operand) [ , ... ] ]
[ "clobber" [ , ... ] ]
]
]);
You must specify an assembler instruction template, plus an operand
constraint string for each operand. The template
specifies the instruction mnemonic, and optionally placeholders for the operands. The
constraint strings specify operand constraints, for example, that
an operand must be in a register (the usual case), or that an operand must be an
immediate value.
Constraint letters and modifiers supported by the compiler are listed in the following tables.
| Letter | Constraint |
|---|---|
c |
A register suitable for use in an indirect jump |
d |
An address register. This is equivalent to @code{r}
unless generating MIPS16 code |
ka |
Registers that can be used as the target of multiply-accumulate instructions |
l |
The @code{lo} register. Use this register to store
values that are no bigger than a word |
x |
The concatenated @code{hi} and
@code{lo} registers. Use this register to store
double-word values |
| Letter | Constraint |
|---|---|
I |
A signed 32-bit constant (for arithmetic instructions) |
J |
Integer zero |
K |
An unsigned 32-bit constant (for logic instructions) |
L |
A signed 32-bit constant in which the lower 32 bits are zero. Such
constants can be loaded using @code{lui} |
M |
A constant that cannot be loaded using @code{lui},
@code{addiu} or @code{ori} |
N |
A constant in the range -65535 to -1 (inclusive) |
O |
A signed 15-bit constant |
P |
A constant in the range 1 to 65535 (inclusive) |
| Letter | Constraint |
|---|---|
R |
An address that can be used in a non-macro load or store. |
| Letter | Constraint |
|---|---|
= |
Means that this operand is write-only for this instruction: the previous value is discarded and replaced by output data |
+ |
Means that this operand is both read and written by the instruction |
& |
Means that this operand is an earlyclobber operand,
which is modified before the instruction is finished using the input
operands. Therefore, this operand may not lie in a register that is used
as an input operand or as part of any memory address |
d |
Second register for operand number n, that is,
%dn.. |
q |
Fourth register for operand number n, that is,
%qn.. |
t |
Third register for operand number n, that is,
%tn.. |