17.2.1 Interrupt Attribute
Use the interrupt attribute to indicate that the specified function is
an interrupt handler. The compiler generates function entry and exit sequences suitable
for use in an interrupt handler when this attribute is present. The generated code
preserves context by either using a shadow register set (SRS) or using generated
software instructions (SOFT) to push context onto the stack.
__attribute__((interrupt([IPLn[SRS|SOFT|AUTO]])))where
n is in the range of 0 through 7,
inclusive.Interrupt Attribute
void __attribute__((interrupt(IPL7SRS))) bambam (void)
{
// interrupt code goes here
}
extern "C" with the
definition, for example:extern "C"
void __attribute__((interrupt(IPL7SRS))) bambam (void)
{
// interrupt code goes here
}Many PIC32 devices allow us to specify, via configuration-bit settings, which interrupt
priority level will use the shadow register set (for example, #pragma config
FSRSSEL=PRIORITY_7). Refer to the device data sheet to determine if your
PIC32 target device supports this feature. This means we must specify which
context-saving mechanism to use for each interrupt handler. The compiler will generate
interrupt function prologue and epilogue code utilizing shadow register context saving
for the IPLnSRS Interrupt
Priority Level (IPL) specifier. It will use software context saving for the
IPLnSOFT IPL
specifier.
Other PIC32 variants may have 8 register sets (1 standard set and 7 shadow register sets) meaning that there are enough shadow register sets for every interrupt priority level. Therefore, you should use the IPLnSRS IPL specifier for every interrupt service routine on these device variants.
The compiler also supports an IPLnAUTO IPL specifier that uses the
run-time value in SRSCTL to determine whether it should use software or
SRS context-saving code. The compiler defaults to using IPLnAUTO when
the IPL specifier is omitted from the interrupt() attribute.
For devices that do not support a shadow register set for interrupt context saving, use IPLnSOFT for all interrupt handlers.
SRS has the shortest
latency and SOFT has a longer latency due to registers saved on the
stack. AUTO adds a few cycles to test if SRS or
SOFT should be used.For IPL7(SRS | SOFT | AUTO), the compiler assumes that nothing can
interrupt priority 7. This means that there is no reason to save EPC or
SRSCtl and that global disabling of interrupts is unnecessary.
The IPLnSAVEALL interrupt priority specifier can be used with the
interrupt attribute. Use this specifier in place of IPLnSOFT to force
software context saving of all software-saved general registers even if they are not
used within the Interrupt Service Routine (ISR). This attribute can be useful for some
RTOS implementations.
The keep_interrupts_masked attribute can be used to modify the behavior
of an interrupt handler. The attribute keeps interrupts masked for the whole function.
Without this attribute, the XC32 compiler re-enables interrupts for as much of the
function as it can. By keeping interrupts masked, support for nested interrupts is
disables. Users can re-enable them as necessary in their own code.
The attribute keep_interrupts_masked can be combined with the
interrupt attribute. This attribute causes the Interrupt Service
Routine (ISR) prologue code to not re-enable interrupts. Application code may then
choose whether and when to re-enable interrupts in the ISR.