16.3 Allocation of Function Code
Code associated with C/C++ functions is normally always placed in the program Flash memory of the target device.
Functions may be located in and executed from RAM rather than Flash by using the
__ramfunc__ and __longramfunc__ macros.
Functions specified as a RAM function will be copied to RAM by the start-up code and all
calls to those functions will reference the RAM location. Functions located in RAM will
be in a different 512MB memory segment than functions located in program memory, so the
longcall attribute should be applied to any RAM function, which
will be called from a function not in RAM. The __longramfunc__ macro
will apply the longcall attribute as well as place the function in
RAM.
#include <sys/attribs.h>
/* function ‘foo’ will be placed in RAM */
void __ramfunc__ foo (void)
{
}
/* function ‘bar’ will be placed in RAM and will be invoked
using the full 32 bit address */
void __longramfunc__ bar (void)
{
}
__longramfunc__ is functionally equivalent to specifying
both __ramfunc__ and __longcall__.