16.9 Inline Functions
By declaring a function inline, you can direct the compiler to integrate
that function’s code into the code for its callers. This usually makes execution faster
by eliminating the function-call overhead. In addition, if any of the actual argument
values are constant, their known values may permit simplifications at compile time, so
that not all of the inline function’s code needs to be included. The effect on code size
is less predictable. Machine code may be larger or smaller with inline functions,
depending on the particular case.
To declare a function inline, use the inline keyword in its declaration,
like this:
inline int
inc (int *a)
{
(*a)++;
}
If you are using the -ansi option, write __inline__
instead of inline. You can also make all “simple enough” functions
inline with the command-line option -finline-functions. The compiler
heuristically decides which functions are simple enough to be worth integrating in this
way, based on an -estimate of the function’s size.
-finline or
optimizations enabled.Certain usages in a function definition can make it unsuitable for inline substitution.
Among these usages are: use of varargs, use of alloca,
use of variable-sized data, use of computed goto and use of nonlocal
goto. Using the command-line option -Winline will
warn when a function marked inline could not be substituted and will
give the reason for the failure.
In compiler syntax, the inline keyword does not affect the linkage of
the function.
When a function is both inline and static, if all calls
to the function are integrated into the caller and the function’s address is never used,
then the function’s own assembler code is never referenced. In this case, the compiler
does not actually output assembler code for the function, unless you specify the
command-line option -fkeep-inline-functions. Some calls cannot be
integrated for various reasons (in particular, calls that precede the function’s
definition cannot be integrated and neither can recursive calls within the definition).
If there is a non-integrated call, then the function is compiled to assembler code as
usual. The function must also be compiled as usual if the program refers to its address,
because that can’t be inlined. The compiler will only eliminate inline
functions if they are declared to be static and if the function
definition precedes all uses of the function.
When an inline function is not static, then the
compiler must assume that there may be calls from other source files. Since a global
symbol can be defined only once in any program, the function must not be defined in the
other source files, so the calls therein cannot be integrated. Therefore, a
non-static inline function is always compiled on its own in the
usual fashion.
If you specify both inline and extern in the function
definition, then the definition is used only for inlining. In no case is the function
compiled on its own, not even if you refer to its address explicitly. Such an address
becomes an external reference, as if you had only declared the function and had not
defined it.
This combination of inline and extern has a similar
effect to a macro. Put a function definition in a header file with these keywords and
put another copy of the definition (lacking inline and
extern) in a library file. The definition in the header file will
cause most calls to the function to be inlined. If any uses of the function remain, they
will refer to the single copy in the library.