3.5.17 How Do I Customize the C Runtime Startup Code?
Some applications may require an application-specific version of the C runtime startup code. For instance, you may want to modify the startup code for an application loaded by a bootloader.
To customize the startup code for your application:
- Start with the default startup code, a copy of which is located in the
pic32m-libs.zip file located
at:
<install-directory>/pic32-libs/Once the file is unzipped, the source code can be found at:
pic32m-libs/libpic32/startup/crt0.S - Make a copy of this crt0.S file, rename it, and add it to your project.
- Change your MPLAB X project to
exclude the default startup code by enabling the “Do not link startup code” under
XC32 xc32-ld Option categories: Libraries page as shown below. When you build your
project, the MPLAB X IDE will build your new application-specific copy of the
startup code rather than linking in the default code.
Figure 3-1. Startup Code Properties Setting 
- You can now edit the assembly code in your new copy of the crt0.S file. The default
source code uses macros defined in the device-specific header files, which are
included by xc.h. These macros define various device specific behavior. Be sure to
take this device-specific code into account when customizing your copy of the
code.
Table 3-1. Device-Specific Macros Device-Specific Macro Description __PIC32_SRS_SET_COUNTDefined to the number of Register Sets implemented on the device. The default startup code uses this value to determine how many register sets to use for $GP-register initialization. __PIC32_HAS_L1CACHEDefined if the device features an L1 cache. __PIC32_HAS_MIPS32R2Defined if the device supports the MIPS32r2 Instruction Set. __PIC32_HAS_MICROMIPSDefined if the device supports the microMIPS compressed Instruction Set. __PIC32_HAS_DSPR2Defined if the device supports the DSPr2 Application-Specific Extension. __PIC32_HAS_FPU64Defined if the device supports the single- and double-precision hardware Floating Point Unit. __PIC32_HAS_SSXDefined if the device does not require initialization of the bus matrix registers in order to support execution from data memory. __PIC32_HAS_MMU_MZ_FIXEDDefined if the device features a Memory Management Unit that should be pre-initialized to a standard SQI and EBI mapping. __PIC32_HAS_INIT_DATADefined if the device requires data initialization by copying from a template located in Flash to RAM.