13.2 Type References
Another way to refer to the type of an expression is with the typeof
keyword. This is a non-standard extension to the language. Using this feature reduces
your code portability.
The syntax for using this keyword looks like sizeof, but the construct
acts semantically like a type name defined with typedef.
There are two ways of writing the argument to typeof: with an expression
or with a type. Here is an example with an expression:
typeof (x[0](1))
This assumes that x is an array of functions; the type described is that
of the values of the functions.
Here is an example with a typename as the argument:
typeof (int *)
Here the type described is a pointer to int.
If you are writing a header file that must work when included in ANSI C programs,
write _ _typeof_ _ instead of typeof.
A typeof construct can be used anywhere a typedef name
could be used. For example, you can use it in a declaration, in a cast, or inside of
sizeof or typeof.
- This declares
ywith the type of whatxpoints to:typeof (*x) y; - This declares
yas an array of such values:typeof (*x) y[4]; - This declares
yas an array of pointers to characters:typeof (typeof (char *)[4]) y;It is equivalent to the following traditional C declaration:
char *y[4];
To see the meaning of the declaration using typeof, and why it might be
a useful way to write, let’s rewrite it with these macros:
#define pointer(T) typeof(T *)
#define array(T, N) typeof(T [N])
Now the declaration can be rewritten this way:
array (pointer (char), 4) y;
Thus, array (pointer (char), 4) is the type of arrays of four pointers
to char.