5.7.7.7 Align-jumps Option
The -falign-jumps=n
option aligns branch targets, where the targets can only be reached by jumping, to the
next power of two greater than n. For instance,
-falign-jumps=32 aligns targets to the next 32-byte boundary;
-falign-jumps=24 aligns targets to the next 32-byte boundary but
only if this can be done by skipping no more than 23 bytes.
The
-fno-align-jumps form of this option is equivalent to
-falign-jumps=1, which implies that the target is not aligned. If
n is not specified or is zero, , a default of
alignment of 1 byte is used, which implies that the target is not aligned. If
n is not a power of 2, the alignment value is
rounded up.
For instance, -falign-jumps=32 aligns targets to the next 32-byte
boundary; -falign-jumps=24 aligns targets to the next 32-byte boundary
but only if this can be done by skipping no more than 23 bytes.
This option is automatically enabled at optimization levels -O2 and
-O3.
If the alignment values specified by -falign-labels is greater than that
specified with this option, then its value is used to align jumps instead.