5.7.7.49 Zero-call-used-regs Option
The -fzero-call-used-regs=choice option instructs the compiler
to zero out a subset of the "call-used" registers associated with each function when
those functions return. Call-used registers are those registers that can be altered by a
function call. This action can enhance program security by reducing the risk of
return-oriented programming (ROP) attacks or preventing information leakage through
registers.
choice argument allows you to select which subset
of call-used registers should be zeroed. The four basic options for
choice are:- skip
- No call-used registers are zeroed.
- used
- Only call-used registers that have been set or referenced in the function are zeroed.
- all
- All call-used registers are zeroed.
used and all options can be further refined with
the following suffixes:- -gpr
- Limits zeroing to general-purpose registers.
- -arg
- Limits zeroing to function argument registers, as defined by the platform’s calling convention.
You can use these suffixes individually or together. If both are used, they must appear
in the above order. For example, used-gpr zeros only general-purpose
call-used registers that have been set or referenced in the function;
used-arg zeros only call-used registers used for function arguments
that have been set or referenced; and used-gpr-arg zeros only
general-purpose call-used registers used for function arguments that have been set or
referenced.
Choices like used-arg, used-gpr-arg,
all-arg, and all-gpr-arg are primarily used for
ROP mitigation.
The compiler's encoding of individual functions can be controlled by the
zero_call_used_regs attribute, which overrides this option. See
Zero_call_used_regs Function Attribute.