5.7.7.28 Lto Option

This -flto option runs the standard link-time optimizer.

When invoked with source code, the compiler adds an internal bytecode representation of the code to special sections in the object file. When the object files are linked together, all the function bodies are read from these sections and instantiated as if they had been part of the same translation unit. Link time optimizations do not require the presence of the whole program to operate.

To use the link-timer optimizer, specify -flto both at compile time and during the final link. For example:
xc32-gcc -c -O3 -flto -mprocessor=32MZ2048ECH100
                                        -mdfp="Microchip/Microchip.PIC32MZ-EC_DFP.1.4.150" foo.c
xc32-gcc -c -O3 -flto -mprocessor=32MZ2048ECH100
                                        -mdfp="Microchip/Microchip.PIC32MZ-EC_DFP.1.4.150" bar.c
xc32-gcc -o myprog.elf -flto -O3 -mprocessor=32MZ2048ECH100
                                        -mdfp="Microchip/Microchip.PIC32MZ-EC_DFP.1.4.150" foo.o bar.o
Another (simpler) way to enable link-time optimization is:
xc32-gcc -o myprog.elf -flto -O3 -mprocessor=32MZ2048ECH100
                                        -mdfp="Microchip/Microchip.PIC32MZ-EC_DFP.1.4.150" foo.c bar.c
Important: Object and library archive files built with LTO enabled are versioned, and there is a strict version check, so those files generated in one version of the compiler might not work with a different version. Additionally, any object or library archive built with LTO enabled can only be used with projects built on the same platform. For example, a library built with LTO on the Windows platform can only be used with other projects that will be built on Windows.

The -fno-lto form of this option does not run the standard link-time optimizer. This is the default action if this option is not specified.