When initializing the SPI, several options need to be specified.
This is done by programming the appropriate control bits (SSPxCON1[5:0] and
SSPxSTAT[7:6]). These control bits allow the following to be specified:
- Host mode (SCK is the clock output)
- Client mode (SCK is the clock input)
- Clock Polarity (Idle state of SCK)
- Data Input Sample Phase (middle or end of data output time)
- Clock Edge (output data on rising/falling edge of SCK)
- Clock Rate (Host mode only)
- Client Select mode (Client mode only)
To enable the serial port, the SSP Enable (SSPEN)
bit must be set. To reset or reconfigure SPI mode, clear the SSPEN bit, re-initialize the
SSPxCONy registers and then set the SSPEN bit. The SDI, SDO, SCK and SS serial port pins are selected with the PPS
controls. For the pins to behave as the serial port function, some must have their data
direction bits (in the TRIS register) appropriately programmed as follows:
- SDI must have corresponding TRIS bit set
- SDO must have corresponding TRIS bit cleared
- SCK (Host mode) must have corresponding TRIS bit cleared
- SCK (Client mode) must have corresponding TRIS bit set
- The RxyPPS and SSPxCLKPPS controls must
select the same pin
- SS must have the
corresponding TRIS bit set
Any serial port function that is not desired may be overridden by programming the corresponding data direction (TRIS) register to the opposite value.
The MSSP consists of a transmit/receive shift (SSPSR) register and a
buffer register (
SSPxBUF). The SSPSR shifts the data in and out of the device, MSb first. The
SSPxBUF holds the data that was written to the SSPSR until the received data is ready. Once
the eight bits of data have been received, that byte is moved to the SSPxBUF register.
Then, the Buffer Full Status (
BF)
bit and the MSSP Interrupt Flag (SSPxIF) bit are set. This double-buffering of the received
data allows the next byte to start reception before reading the data that was just
received. Any write to the SSPxBUF register during transmission/reception of data will be
ignored and the Write Collision Detect (
WCOL)
bit will be set. User software must clear the WCOL bit to allow the following write(s) to
the SSPxBUF register to complete successfully.
When the application software is expecting to receive valid data,
the
SSPxBUF
must be read before the next byte of data to be transferred is written to the SSPxBUF. The
BF bit indicates when SSPxBUF has been loaded with the received data
(transmission is complete). When the SSPxBUF is read, the BF bit is cleared. This data may
be irrelevant if the SPI is only a transmitter. Generally, the MSSP interrupt is used to
determine when the transmission/reception has completed. If the interrupt method is not
going to be used, then software polling can be done to ensure that a write collision does
not occur.
Important: The SSPSR is not directly readable or writable and can only be accessed
by addressing the SSPxBUF register.