19.5 CRC Interrupt
The CRC module will generate an interrupt when the BUSY bit transitions from
‘1’ to ‘0’. The
CRC Interrupt Flag (CRCIF) bit of the corresponding PIR register
will be set every time the BUSY bit transitions, regardless of
whether or not the CRC Interrupt Enable (CRCIE) bit has been
set. The CRCIF bit must be cleared by software by the user. If
the user has the CRCIE bit set, then the CPU will jump to the
Interrupt Service Routine (ISR) every time that the CRCIF bit is
set.