4 Power Supply and Monitor

Power supply, Power Monitor.

Power SupplyPower Monitor

4.1 Power Supply

Figure 4-1. Power Supply Overview
Board OverviewUSB BridgePower MuxCurrent Limiting SwitchPower MonitorVoltage Reference3.3V Bridge Regulator3.3V Target Regulator
Important: The Explorer powers the CNANO at 3.3V, and all the pins connected to the CNANO socket are designed for use with 3.3V I/O pins.
The Explorer’s power supply features:
  • Dedicated 3.3V regulator to power the CNANO and 3.3V peripherals
  • 5V peripherals powered directly by USB voltage
  • A power multiplexer allows power supplied from the on-board USB-C® connector or the CNANO
  • A current limiting switch with a soft start to protect the board, the current limit set at 2A
  • On-board power monitoring for voltage and current measurement with four channels
Table 4-1. Power Domain Specifications
Power DomainVnomVmin - VmaxImax
P5V05.0V4.4–5.5V2.0A
P3V33.30V3.22–3.38V1.2A
CNANO P3V33.30V3.22–3.38V1.2A
BRIDGE P3V33.30V3.23–3.37V150 mA

4.1.1 Power Sources

The two main power sources are:
  • The USB connector on the CNANO
  • The USB-C® connector on the Explorer
Current limitations:
  • The CNANO’s VBUS output has a current limitation of 500 mA
  • The Explorer’s USB-C® connector can sink different amounts of current based on the USB source (up to 3.0A from a USB-C® source)
  • Both USB inputs are fed into a power multiplexer, with output current limited to 2.0A
Info: If both USB connectors are powered, the current is sourced through the Explorer's USB-C® connector.
Figure 4-2. Power MUX Overview
Board OverviewPower DomainsUSB Bridge

4.1.2 Power Domains

There are four main power domains on the Explorer:
  • P5V0
  • P3V3
  • CNANO P3V3
  • BRIDGE P3V3

CNANO P3V3 is powered by the same regulator as P3V3, separated for dedicated power measurement of the CNANO. It powers the CNANO’s external power input. Refer to CNANO Power Configuration for more information.

Table 4-2. Peripherals Connected to the Different Power Domains
Power DomainPower Measurement ChannelPeripheral
CNANO P3V3CH1 (uA), CH4 (mA)Connected CNANO
P3V3CH2 (mA)Touch controller
I/O expander 2 + button LEDs
I/O expander 1 + LED row
I2C EEPROM
Secure Element
Proximity and ambient light sensor (digital circuitry)
Temperature sensor
OLED display
SPI EEPROM
DAC
Voltage reference
Microphone circuit
Speaker circuit
Potentiometer
mikroBUS™ socket (3.3V pin)
MicroSD card socket
Grove and Qwiic®connector
P5V0CH3 (mA)RGB LED
Digital addressable LEDs
Servomotor circuit
Proximity and ambient light sensor (internal LED)
mikroBUS™ socket (5V pin)
BRIDGE P3V3-Power monitor circuit
USB bridge circuit
Figure 4-3. Power Domains Overview
Power MuxCurrent Limiting SwitchBoard Overview

4.1.3 Current Limiting Switch

A MIC2008 current limiting switch with an adjustable slew rate is mounted on the board to prevent large inrush currents. The switch has been configured with a current limit of 2.0A by selecting resistor R500 to be 120Ω.
Info: MIC2008 current limit range: 0.2–2.0A. See the MIC2008 data sheet for more information
Figure 4-4. Current Limiting Switch
Power Mux3.3V Target RegulatorBoard overview

4.1.4 CNANO Power Configuration

The Explorer supplies the CNANO with a fixed 3.3V. When connected to the Explorer, the on-board regulator of the CNANO is disabled by pulling the VOFF pin low, ensuring no logic level mismatches between the CNANO and the Explorer.

Info: The CNANO's on-board debugger is only powered when the CNANO USB is connected to power.
Important: When connected to the Explorer, the adjustable target voltage feature of the CNANO is disabled.
Figure 4-5. Power Configuration of the Connected CNANO
Board OverviewPower MuxCurrent Limiting SwitchUSB Bridge3.3V Target Regulator

4.2 Power Monitor

4.2.1 Getting Started with Power Monitor

The on-board PAC1944 quad-channel power monitor circuit allows tracking of the power consumption of peripherals on the Explorer. The measurement data can be accessed through the USB bridge MCP2221A.

To read and visualize power data, download and install the PAC194x/PAC195x Demo Application.
Figure 4-6. PAC194x/PAC195x Demo Application
Open the application and perform the following steps to get started:
  1. Configure the sense resistor value:
    1. Channel 1: 51000
    2. Channel 2: 75
    3. Channel 3: 50
    4. Channel 4: 220
  2. Start Acquisition.
  3. Press "Show Plots" to visualize the data.
Important: While using the demo application set the I2C slide switch to the "NC" position, which isolates the PAC1944 and MCP2221A from the rest of the Explorer’s I2C bus.

4.2.2 Power Measurement Channels

The four PAC1944 measurement channels measure three of the four main power domains on the Explorer:
  • P5V0 (CH3)
  • P3V3 (CH2)
  • CNANO P3V3 (CH1 and CH4)
Figure 4-7. Measurement Channels
Power MuxCurrent Limiting Switch3.3V Target RegulatorBoard Overview
Table 4-3. Measurement Channel Specifications
Default Power DomainChannelCurrent Sense RangeCurrent Sense ResolutionSense Resistor
P5V0 (mA)CH3≤ 2.00A30.5 μA0.050Ω
P3V3 (mA)CH2≤ 1.33A20.3 μA0.075Ω
CNANO P3V3 (mA)CH4≤ 455 mA6.94 μA0.220Ω
CNANO P3V3 (μA)CH1≤ 1.96 mA29.9 nA51.0Ω
Tip: To identify which peripherals are powered by each power domain, see Table 4-2.

Measure CNANO P3V3 Power

CH1 and CH4 measure current to the CNANO P3V3 power domain.
  • CH1 for µA measurements
  • CH4 for mA measurements
The user can change which channel is in use by placing or removing the pin jumper on pin header J506.
Important: The sense resistor for CH1 is 51Ω. Currents above 2 mA will cause a significant voltage drop in the voltage supplied to the attached CNANO.
Figure 4-8. Currents Above 2 mA (CH1 bypassed)
Figure 4-9. Currents Below 2 mA (CH1 connected)

Measure External Power

CH1 and CH3 can be disconnected from their default connections to measure current from external sources.

Warning: Remember to connect the GND from the Explorer to the GND of the external source. Do not apply voltages above 9V to the current measurement channels.
Figure 4-10. Connect External Source to CH1 (µA)
Figure 4-11. Connect External Source to CH3 (mA)

4.2.3 Quad Channel Precision Power Monitor

Feature overview:
  • High-side current monitor with four channels
  • 100 mV full-scale range
  • 0-9V full-scale range
  • 16-bit resolution
  • On-chip accumulation of 30-bit power results from energy measurement

The PAC1944 may also be accessed by the microcontroller on the CNANO using the I2C bus.

Important: Set the I2C slide switch to the "MCP2221A" position to connect the PAC1944 and MCP2221A to the rest of the I2C bus on the board.
Figure 4-12. Power Monitor Overview
Board OverviewRemapping AreaI2C Bus