4.2 Statement Formats
Valid statement formats are shown in Table 4-3.
The label field is optional and, if present,
         should contain one identifier. A label can appear on a line of its own, or precede a
         mnemonic as shown in the second format.
The third format is only legal with certain assembler directives, such as
            MACRO, SET and EQU. The
               name field is mandatory and should contain one
         identifier.
If the assembly source file is first processed by the preprocessor, then it can also contain lines that form valid preprocessor directives. See Preprocessor Directives for more information on the format for these directives.
There is no limitation on what column or part of the line in which any part of the statement should appear.
| Format # | Field1 | Field2 | Field3 | Field4 | 
|---|---|---|---|---|
| Format 1 | label: | |||
| Format 2 | label: | mnemonic | operands | ; comment | 
| Format 3 | name | pseudo-op | operands | ; comment | 
| Format 4 | ; comment
                     only | |||
| Format 5 | empty line |