4.9 Assembler Directives
Assembler directives, or pseudo-ops, are used in a similar way to
         instruction mnemonics. With the exception of PAGESEL and
            BANKSEL, these directives do not generate instructions. The
            DB, DW and DDW directives place data
         bytes into the current psect. The directives are listed in the following sections. 
| Directive | Purpose | 
|---|---|
ALIGN | Aligns output to the specified boundary. | 
ASMOPT | Controls whether subsequent code is optimized by the assembler. | 
BANKISEL | Generates code to select bank of operand for indirect access on some devices. | 
BANKSEL | Generates code to select bank of operand. | 
CALLSTACK | Indicates the call stack depth remaining. | 
COND | Controls inclusion of conditional code in the listing file. | 
CONFIG | Specifies configuration bits. | 
DABS | Defines absolute storage. | 
DB | Defines constant byte(s). | 
DDW | Defines double-width constant word(s). | 
DEBUG_SOURCE | Controls debug information. | 
DLABS | Define linear-memory absolute storage. | 
DS | Reserves storage. | 
DW | Defines constant word(s). | 
ELSE | Alternates conditional assembly. | 
ELSIF | Alternates conditional assembly. | 
ENDIF | Ends conditional assembly. | 
END | Ends assembly. | 
ENDM | Ends macro definition. | 
EQU | Defines symbol value. | 
ERROR | Generates a user-defined error. | 
EXPAND | Controls expansion of assembler macros in the listing file. | 
EXTRN | Links with global symbols defined in other modules. | 
FILE | Indicates the source file that contains the assembly code following. | 
FNADDR | Indicates a routine's address has been taken. | 
FNARG | Indicates calls in a routine's arguments. | 
FNBREAK | Breaks links in the call graph. | 
FNCALL | Indicates call hierarchy. | 
FNCONF | Indicates call stack settings. | 
FNINDIR | Indicates indirect calls made by routines. | 
FNSIZE | Indicates the size of a routines auto and parameter objects. | 
FNROOT | Indicates the root of a call tree. | 
GLOBAL | Makes symbols accessible to other modules or allow reference to other global symbols defined in other modules. | 
IF | Conditional assembly. | 
INCLUDE | Textually includes the content of the specified file. | 
IRP | Repeats a block of code with a list. | 
IRPC | Repeats a block of code with a character list. | 
LINE | Indicates the line number of the current source file that contains the assembly code following. | 
LIST | Defines options for listing file. | 
LOCAL | Defines local tabs. | 
MACRO | Macro definition. | 
MESSG | Generates a user-defined advisory message. | 
NOCOND | Controls inclusion of conditional code in the listing file. | 
NOEXPAND | Controls expansion of assembler macros in the listing file. | 
NOLIST | Disable assembly listing. | 
ORG | Sets location counter within current psect. | 
PAGELEN | Specifies the length of the listing file page. | 
PAGESEL | Generates set/clear instruction to set PCLATH bits for this page. | 
PAGEWIDTH | Specifies the width of the listing file page. | 
PROCESSOR | Defines the particular chip for which this file is to be assembled. | 
PSECT | Declares or resumes program section. | 
PUBLIC | Makes non-EXTRN symbols accessible to other
                     modules or allow reference to other global symbols defined in other
                     modules. | 
RADIX | Specifies radix for numerical constants. | 
REPT | Repeats a block of code n times. | 
SET | Defines or re-defines symbol value. | 
SIGNAT | Defines function signature. | 
SUBTITLE | Specifies the subtitle of the program for the listing file. | 
TITLE | Specifies the title of the program for the listing file. | 
WARN | Generates a user-defined warning. |