6.1.31 Fixupoverflow Linker Option
The --fixupoverflow=action option
specifies how the linker will respond should it encounter an overflow when fixing up a
symbol.
Fixup is the process of replacing symbolic references in code with an actual value once
psects have been located in memory and the address or value of symbols have been
resolved. If the linker determines that the value of a symbol is too large to fit into
the space reserved for it in the program image, then this is known as a fixup
overflow. The default
action of the linker when encountering a fixup overflow in hand-written assembly
programs built with the pic-as driver is to place warning markers
in the assembly list file where possible.
--fixupoverflow option customizes the action taken by the linker
when a fixup overflow situation is encountered, as described by the
action arguments in the following table.| Action | Response |
|---|---|
error | Trigger an error message |
warn | Truncate the value to fit and trigger a warning message. |
lstwarn | Truncate the value to fit and insert a warning marker into the
assembly list file where the overflow occurred. (the default response when used
with pic-as) |
ignore | Truncate the value to fit and continue with no notification of the fact. |
The warn and lstwarn actions can both be selected with
this option, in which case they must be separated by a colon (:), for
example --fixupoverflow=warn:lstwarn.
-Wa,-a
assembler option and the lstwarn action has
been requested, a warning message will be inserted into the list file before the
instruction or directive that contains the symbol being fixed up. The message will
appear similar
to:13 003FF4 6F14 movwf _bar,b
14 003FF6
warning: (2090) fixup overflow storing 0x202 in 1 byte
5102 movf _foo,w,bwhich shows an
overflow associated with the symbol _foo. In this instance, the symbol
has been resolved to the value 0x202, but there are only 7 bits in the
movf instruction to hold the address offset of the file register
being accessed. The linker has truncated the value 0x202 to a 7-bit quantity (0x02) and
inserted this into the program image forming the opcode 0x5102.If warning messages are inserted into a list file, a single advisory message will be
issued by the assembler for each affected list file to alert
you to this action. If the lstwarn action was specified, but an
assembly list file was not actually requested, then an alternate warning message will be
issued by the assembler.
Fixup overflows in hand-written assembly programs might
indicate some sort of error in how the code was written or linked. It is commonly
associated with the address of symbols in PIC programs that have not been masked to
remove the banking or paging information. In this case, if you do not wish to mask
addresses manually (see the Address Masking section in this guide), this option can be
used to truncate the addresses and allow the program to build. It should be stressed
that this option will, however, suppress the error message associated with any fixup
overflow. It is recommended that an action of warn, or
lstwarn be used so that you can monitor which instructions are
affected. If there is some other erroneous situation in your program, using this option
will in no way address the underlying issue.