6.1.22 S: Place Upper Address Limit On Class
A class of psects can have an upper address limit associated with it.
The following example of the -Sclasslimit[,bound]= option
places a limit on the maximum address of the CODE class of psects to
one less than 400h.
-SCODE=400h
Note that to set an upper limit to a psect, this must be set in
assembler code using the psect limit flag, (see Limit Flag).
If the bound (boundary) argument is used, the
class of psects will start on a multiple of the bound address. This example below places
the FARCODE class of psects at a multiple of 1000h, but with an upper
address limit of 6000h.
-SFARCODE=6000h,1000h