4.9.7 Config Directive

The CONFIG directive allows the configuration bits (or fuses) and ID-location registers to be specified in the assembly source file. Configuration bits, or fuses, are used to set up fundamental device operation, such as the oscillator mode, watchdog timer, programming mode and code protection. These bits must be correctly set to ensure your program executes correctly.

The directive has the following forms:

CONFIG setting = value
CONFIG register = literal_value
Here, setting is a configuration setting descriptor (e.g., WDT) and value can be either a textual description of the desired state (e.g., OFF) or a numerical value. Either the setting or value tokens or the setting = value expression can be surrounded by either double or single quotes to protect them from any macro substitution performed by the preprocessor, for example:
CONFIG "WDT = ON"         ;turn on watchdog timer
CONFIG "FEXTOSC" = "ECH"  ;external clock oscillator mode, high power PFM
CONFIG WDTPS = 0x1A       ;specify the timer postscale value
Some value tokens that appear to be purely numerical are in fact a textual description of the value, for example in the following:
config WDTPS = 32
the 32 token is a textual description for some devices that indicates a watchdog timer post-scale of 1:32, not the number 32. In such a case, it might not be the number 32 that is programmed into the relevant bits of the configuration register. The assembler will first check if value represents a predefined string and, only if that is not the case, assume it represents a numerical constant, which will then be subject to the same constraints as other numerical constant operands.

You should never assume that the OFF and ON tokens used in configuration macros equate to 0 and 1, respectively, as that is often not the case.

The register field is the name of a configuration or ID-location register, and this must always be used with a value that is a numerical constant, for example:
CONFIG CONFIG1L = 0x8F

The available setting, register and value fields are documented in the chipinfo file relevant to your device (i.e. pic_chipinfo.html and pic18_chipinfo.html) and that are located in the docs directory of your selected DFP. Click the link to your target device and the page will show you the settings and values that are appropriate with this pragma. Review your device data sheet for more information.

One CONFIG directive can be used to set each configuration setting; alternatively, several comma-separated configuration settings can be specified by the same directive. The directive can be used as many times as required to fully configure the device.

The following example shows a configuration register being programmed as a whole and programmed using the individual settings contained within that register.
; PIC18F67K22
; VREG Sleep Enable bit : Enabled
; LF-INTOSC Low-power Enable bit : LF-INTOSC in High-power mode during Sleep
; SOSC Power Selection and mode Configuration bits : High Power SOSC circuit selected
; Extended Instruction Set : Enabled
CONFIG RETEN = ON, INTOSCSEL = HIGH, SOSCSEL = HIGH, XINST = ON

; Alternatively
CONFIG CONFIG1L = 0x5D

; IDLOC @ 0x200000
CONFIG IDLOC0 = 0x15

All the bits in the Configuration Words should be programmed to prevent erratic program behavior. Do not leave them in their default/unprogrammed state. Not all Configuration bits have a default state of logic high; some have a logic low default state. Consult your device data sheet for more information.

Do not mix C config pragmas and assembly config directives in the same program. Choose one method to program the entire set of configuration words.

If you are using MPLAB X IDE, take advantage of its built-in tools to assist you obtain the required config directives. See the MPLAB® X IDE User’s Guide for a description and use of the Configuration Bits window.