3.2.4 I2C Interface
The I2C source streams the raw values received on the I2C interface. For further details on the physical part of the I2C interface, see the user guide of the debug tool to be used to sample the I2C data.
The I2C Configuration options are displayed under the DGI section of the Data Sources (left) pane. When an I2C connection is selected, the I2C settings are displayed in the lower section of this pane.
| Field Name | Values | Usage |
|---|---|---|
| Speed | 0 | The expected operation speed of the interface in Hertz helps the client device adjust the timings. Up to 400 kHz is supported. |
| Address | 1 | Address of the client device. |
| Kit-side Timestamping | Check to enable | Target timestamping. |