3.3.6 Threshold
Defines the detected Threshold. When a button is touched, the delta for that button increases. The button will report as touched when the touch delta value is higher than the button’s Threshold. Configuring the Threshold to 50~70% of the touch delta is recommended. It is good to start with the default value and adjust by monitoring the touch delta value. Threshold, in addition to the Gain setting, can be used to set the sensitivity of each button.
Steps to Configure Threshold
- The Threshold value for
Button[n] can be updated by writing in Channel Threshold (THRESHOLD[n])
register.Note: Prior to modifying the register, ensure that the Easy Tune function is disabled. Refer to the “Easy Tune” feature for more information.
- Saving the Settings
(optional):
- Writing
1
in DEVCTRL.SAVE to save the configuration.
- Writing