27.1 Overview
The Direct Memory Access Controller (DMAC) contains both a Direct Memory Access engine and a Cyclic Redundancy Check (CRC) engine. The DMAC can transfer data between memories and peripherals, and thus off-load these tasks from the CPU. It enables high data transfer rates with minimum CPU intervention, and frees up CPU time. With access to all peripherals, the DMAC can handle automatic transfer of data between communication modules.
The DMA part of the DMAC has several DMA channels which all can receive different types of transfer triggers to generate transfer requests from the DMA channels to the arbiter, see also the Block Diagram. The arbiter will grant one DMA channel at a time to act as the active channel. When an active channel has been granted, the fetch engine of the DMAC will fetch a transfer descriptor from the SRAM and store it in the internal memory of the active channel, which will execute the data transmission.
An ongoing data transfer of an active channel can be interrupted by a high-priority DMA channel. The DMAC will write back the updated transfer descriptor from the internal memory of the active channel to SRAM and grant the high- priority channel permission to start the transfer as the new active channel. Once a DMA channel completes its transfer, interrupts and events can be generated optionally.
The DMAC has the following four bus interfaces:
- Data transfer bus – Used for performing the actual DMA transfer.
- AHB/APB Bridge bus – Used when writing and reading the I/O registers of the DMAC.
- Descriptor fetch bus – Used by the fetch engine to fetch transfer descriptors before data transfer can be started or continued.
- Write-back bus – Used to write the transfer descriptor back to SRAM.
All buses are AHB host interfaces except the AHB/APB Bridge bus, which is an APB client interface.
The CRC engine can be used by software to detect accidental errors in the transferred data and to take corrective action, such as requesting the data to be sent again or simply not using the incorrect data.