The Bootloader has the Fuse settings
set to default except below fuse bits
The Bootloader region size
(4096 Bytes) is specified using the BOOTPROT fuse bit. BOOTPROT = 0x10.
The Bootloader region is
protected by setting the SULCK configuration at production to 0x6 (SULCK.BS
= 0).
The Fuse settings can be changed in
following ways:
The Bootloader provides a
separate command to program the Fuse Bits received from the host. Refer to
the Bootloader protocol documentation and respective host utility
documentation for more information.
The application can check the
Fuse bits during the boot-up, then program any change required using the
NVMCTRL peripheral.
Fuse settings are placed in a higher
memory location in the Flash (User Row and BOCOR Row). The Fuse settings need to be
disabled for the application project, which will be boot-loaded, as the size of the
binary file becomes too large when the fuse settings are enabled.
When updating the Bootloader itself,
make sure that the fuse settings for the Bootloader application are also
disabled.
For PIC32CM LS00/LS60:
Proper fuse settings required
by the application have to be sent along with application binary.
Peripherals used by the
Bootloader (SERCOM5, SERCOM2, BOOT Pin) should not be configured as
Non-Secure while updating the Fuse settings.
When WDT is enabled from the
Fuse Settings, the bootloader refreshes the WDT at intervals to avoid reset.
Therefore, the WDT peripheral should not be configured as Non-Secure if it
is enabled through Fuse settings.
DS60001615L
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.