4.16.6 PLL Controls
The PMC embeds 4 PLLs that are controlled by the PMC_PLL_CTRL0, PMC_PLL_CTRL1, PMC_PLL_SSR, PMC_PLL_ACR and PMC_PLL_UPDATE registers. Each PLL is accessed in read or write through its index as defined in the table below, corresponding to the register field PMC_PLL_UPDT.ID. At any time, PLL_CTRL0, PLL_CTRL1 and PLL_ACR reflect the controls for the PLL with index PMC_PLL_UPDT.ID. When the UPDATE bit is set in PMC_PLL_UPDT, the PLL of index PMC_PLL_UPDT.ID is updated with the content of registers PLL_CTRL0, PLL_CTRL1 and PLL_ACR.
Each PLL is fed by either the MAINCK or the main crystal oscillator and has a constraint on the frequency it can generate on its clock output. Refer to the section “Electrical Characteristics”.
| Index | PLL Name | Clock Name | PLL Clock Source | Usage Example |
|---|---|---|---|---|
| 0 | PLLA | PLLACK | MAINCK | CPU_CLK and MCK clock sources |
| 1 | UPLL | ULLCK | MAIN XTAL OSC | UTMI clock source |
| 2 | AUDIOPLL | AUDIOPLLCK | MAIN XTAL OSC | AUDIOCLK output clock source |
| 3 | LVDSPLL | LVDSPLLCK | MAIN XTAL OSC | LVDS clock source |
| 4 | PLLADIV2 | PLLADIV2CK | MAINCK | Generic clocks source |