9.4.6.10.1 Input-Output Transfer Functions
The ADC can be configured to operate in the following input voltage modes:
- Single-Ended—ADC_CCR.DIFFx = 0 and ADC_PDR.PDIFFx = 0. This is the default mode after a reset.
- Differential—ADC_CCR.DIFFx = 1 and ADC_PDR.PDIFFx = 0 (see the figure below). In Differential mode, the ADC requires differential input signals having a VDD/2 common mode voltage (refer to the section “Electrical Characteristics”).
- • Pseudo-Differential—ADC_PDR.PDIFFx = 1. In Pseudo-Differential mode, one of the analog pins is used as the negative input of the ADC (see table Input Pins and Channel Numbers in Pseudo-Differential Mode). The ADC samples the other analog inputs with respect to this one. The common mode input range is 0 to VDD (refer to the section “Electrical Characteristics”).
The following equations provide the unsigned ADC input-output transfer function in each mode(1). With signed conversions (see field ADC_EMR.SIGNMODE), subtract 2047 from the ADC_LCDR.DATA value given below. Note that the Single-Ended mode introduces a x2 gain compared to the Pseudo-Differential mode.
In the formula, REFP = VREFP, REFN = VREFN.
Single-Ended mode:
Differential mode:
Pseudo-Differential mode:
If ADC_MR.ANACH is set, the ADC can manage both differential channels and single-ended channels. If ADC_MR.ANACH is cleared, the parameters defined in ADC_CCR are applied to all channels.
The following tables provide the internal positive and negative ADC inputs assignment with respect to the programmed mode (ADC_CCR.DIFFx and ADC_PDR.PDIFFx).
For example, if Differential mode is required on channel 0, input pins AD0 and AD1 are used. In this case, only channel 0 must be enabled by writing a 1 to ADC_CHER.CH0.
| Internal ADC Inputs (VIN+, VIN-) | Channel Number | ||
|---|---|---|---|
| Single-Ended Mode | Differential Mode | Single-Ended Mode | Differential Mode |
| AD0, ADVREFN | AD0, AD1 | CH0 | CH0 |
| AD1, ADVREFN | – | CH1 | |
| AD2, ADVREFN | AD2, AD3 | CH2 | CH2 |
| AD3, ADVREFN | – | CH3 | |
| AD4, ADVREFN | AD4, AD5 | CH4 | CH4 |
| AD5, ADVREFN | – | CH5 | |
| AD6, ADVREFN | AD6, AD7 | CH6 | CH6 |
| AD7, ADVREFN | – | CH7 | |
In Pseudo-Differential mode, inputs are managed by a 8/2:1-channel analog multiplexer. See the table below.
| Internal ADC Inputs (VIN+, VIN-) | Channel Number |
|---|---|
| AD0, AD7 | CH0 |
| AD1, AD7 | CH1 |
| AD2, AD7 | CH2 |
| AD3, AD7 | CH3 |
| AD4, AD7 | CH4 |
| AD5, AD7 | CH5 |
| AD6, AD7 | CH6 |
| GNDANA, AD7 | CH7 |