25.6.2.1 Initialization
The following DMAC registers are
enable-protected, meaning that they can only be written when the DMAC is disabled
(CTRL.DMAENABLE=0):
- Descriptor Base Memory Address register (BASEADDR)
- Write-Back Memory Base Address register (WRBADDR)
The following DMAC bit is enable-protected,
meaning that it can only be written when both the DMAC and CRC are disabled
(CTRL.DMAENABLE=0 and CTRL.CRCENABLE=0):
- Software Reset bit in Control register (CTRL.SWRST)
The following DMA channel register is
enable-protected, meaning that it can only be written when the corresponding DMA channel is
disabled (CHCTRLA.ENABLE=0):
- Channel Control B (CHCTRLB) register, except the Command bit (CHCTRLB.CMD) and the Channel Arbitration Level bit (CHCTRLB.LVL)
The following DMA channel bit is enable-protected, meaning that it can only be written when the corresponding DMA channel is disabled:
- Channel Software Reset bit in Channel Control A register (CHCTRLA.SWRST)
The following CRC registers are
enable-protected, meaning that they can only be written when the CRC is disabled
(CTRL.CRCENABLE=0):
- CRC Control register (CRCCTRL)
- CRC Checksum register (CRCCHKSUM)
Enable-protection is denoted by the "Enable-Protected" property in the register description.
Before the DMAC is enabled it must be configured, as outlined by the following steps:
- The SRAM address of where the descriptor memory section is located must be written to the Description Base Address (BASEADDR) register
- The SRAM address of where the write-back section should be located must be written to the Write-Back Memory Base Address (WRBADDR) register
- Priority level x of the arbiter can be
enabled by setting the Priority Level x Enable bit in the Control register
(CTRL.LVLENx=
1)
Before a DMA channel is enabled, the DMA channel and the corresponding first transfer descriptor must be configured, as outlined by the following steps:
- DMA channel configurations
- The channel number of the DMA channel to configure must be written to the Channel ID (CHID) register
- Trigger action must be selected by writing the Trigger Action bit group in the Channel Control B register (CHCTRLB.TRIGACT)
- Trigger source must be selected by writing the Trigger Source bit group in the Channel Control B register (CHCTRLB.TRIGSRC)
- Transfer Descriptor
- The size of each access of the data transfer bus must be selected by writing the Beat Size bit group in the Block Transfer Control register (BTCTRL.BEATSIZE)
- The transfer descriptor must be made valid by writing a one to the Valid bit in the Block Transfer Control register (BTCTRL.VALID)
- Number of beats in the block transfer must be selected by writing the Block Transfer Count (BTCNT) register
- Source address for the block transfer must be selected by writing the Block Transfer Source Address (SRCADDR) register
- Destination address for the block transfer must be selected by writing the Block Transfer Destination Address (DSTADDR) register
If CRC calculation is needed, the CRC engine must be configured before it is enabled, as outlined by the following steps:
- The CRC input source must selected by writing the CRC Input Source bit group in the CRC Control register (CRCCTRL.CRCSRC)
- The type of CRC calculation must be selected by writing the CRC Polynomial Type bit group in the CRC Control register (CRCCTRL.CRCPOLY)
- If I/O is selected as input source, the beat size must be selected by writing the CRC Beat Size bit group in the CRC Control register (CRCCTRL.CRCBEATSIZE)