1.2 Hardware Prerequisites
- ATA8510 Curiosity Board Kit (EV82M22A)
- WBZ451HPE Curiosity Board (EV79Y91A)(1)
- SAM C21 Xplained Pro Evaluation Kit (ATSAMC21-XPRO)(2)
- mikroBUS™ Adapter (ATMBUSADAPTER-XPRO)(2)
- Type-A USB to Type-C™ USB Cable
- ATMEL-ICE Programmer (ATATMEL-ICE) or MPLAB® PICkit™ 5 In-Circuit Debugger (PG164150)
Note:
- If using ATA8510 Curiosity Board in the Host mode with WBZ451HPE Curiosity Board as host.
- If using ATA8510 Curiosity Board in the Host mode with SAM C21 Xplained Pro Evaluation Kit as host.
- For more details on the host boards supported by the ATA8510 Curiosity Board, refer to the Example Application section in the ATA8510 Application Developer's Guide.