2.1 Kit Contents
The EV82M22A (ATA8510 Curiosity Board) Kit contains the following:
- ATA8510 Curiosity Board
Note:
- To evaluate sub-GHz TX/RX functionality, obtain two identical kits. Designate one kit as the transmitter and the other as the receiver. For more details, refer to the steps in the ATA8510 Curiosity Board Out-of-the-Box Demo.
- If any of the above items are missing in the kit, go to http://support.microchip.com or contact your local Microchip Sales office via the Global Sales and Distribution page.