3.6 System Lock
The MTCH9010 liquid detector provides a System Lock mechanism that saves the parameters configured through the Enhanced Configuration mode in the Nonvolatile Memory (NVM) and restores the settings at every start-up. Enable this feature at the next start-up after the Enhanced Configuration and calibration process.
The parameters configured using the Enhanced Configuration mode are stored in the NVM at two memory locations for redundancy purposes. The application will load the parameters from the first memory location and use the second memory location only if the loading fails.
The SYS_LK digital input pin controls the usage of the System Lock mode. The following table shows the correspondence between the SYS_LK pin voltage and System Lock settings:
| Voltage on SYS_LK Pin | System Lock |
|---|---|
| 0V | Enabled |
| VDD | Disabled |