7 Appendix: Running the Tcl Script
(Ask a Question)Tcl scripts are provided in the www.microchip.com/en-us/application-notes/an4723.
To run Tcl, perform the following steps:
- Launch the Libero software.
- From the menu bar, click .
- In the downloaded directory
mpfs_an4723_v20xxpx_df, locate and select thescript.tclfile. - To execute the selected Tcl script, click Run.
After a successful execution of the Tcl script, the Libero project is created within the top directory of mpfs_an4723_v20xxpx_df. You can verify the process by reviewing the log file, see mpf_an4723_v20xxpx_df_log.
For more details about the folder structure and details of the Tcl scripts and commands, see the TCL_Scripts_readme.txt file and the
Tcl Commands Reference Guide
. Contact Technical Support team, for any queries about running the Tcl script.