16.5.1 Boot Configuration Word
- To configure the IO Set where the external memories used to boot are connected (see Hardware and Software Constraints for a description of the IO sets)
- To disable the boot on selected memories
- To configure the UART port used as a terminal console
- To configure the JTAG pins used for debug
See the section Boot Configuration Word for a detailed description of all the bitfields in this word.
By default, the value of this word is 0x0.
For MRL A and B parts, the ROM code does not try to detect a valid bootable software in any external memory, and runs directly the SAM-BA monitor. See the figure NVM Bootloader Program Description for MRL A and MRL B Parts.
For MRL C parts, the ROM code only tries to boot on SDMMC1 and SDMMC0 memory interfaces and then run the SAM-BA monitor. See the figure NVM Bootloader Program Description for MRL C Parts.
- The fuse bit DISABLE_BSCR must not be set (default value).
- The Boot Sequence Controller Configuration register (BSC_CR) must have the BUREG_VALID bit set and indicate in BUREG_INDEX which register has to be used.
The backup registers (“BUREG”) can be used to test several boot configuration options, including the Secure Boot mode, without burning fuses.