9 Pulse-Width Modulation (PWM)
Note: For PWM that depends on TMR2, see the Capture/Compare/PWM
(CCP) section.
The 16-bit PWM peripheral is fully stand-alone, meaning it does not utilize another system timer, unlike CCP, which depends on TMR2. There are five operating modes for generating PWM:
- Left-Aligned
- Right-Aligned
- Center-Aligned
- Variable Aligned
- Compare
These modes change how the count is used to generate the output. Inside each instance are slices, each containing two outputs. The outputs share a mutual frequency but have their duty cycle registers. Additionally, the peripheral is double-buffered for smooth output changes and can synchronize with other PWM instances.