1.17 PIT64B Periodic Interrupt
This application shows how to use PIT64B counter in interrupt mode.
Description
This application toggles an LED based on the PIT64B interrupt. Every time the PIT64B counter expires the LED toggles.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/pit64b/period_change.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a7d65_curiosity.X | MPLABX project for SAMA7D65 Curiosity Board |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a7d65_curiosity.X | SAMA7D65 Curiosity Board |
Setting Up SAMA7D65 Curiosity Board
- Connect the USBA port J3 on the board to the computer using a Type-C USB cable (to power the board)
Running the Application
- Build and run the application using its IDE
- Press SW2 switch to start/stop timer
- LED toggles at a fixed rate when timer is on and stops toggling when timer is off
- Press SW4 switch to change the timer period
- When timer period is changed LED toggle rate is changed
- Timer period cycles between 250ms, 500ms, 750ms and 1000ms
| Board | SW2 | SW4 | LED |
|---|---|---|---|
| SAMA7D65 Curiosity Board | USER | RESET | RGB_LED (Blue) |