1.11 FLEXCOM TWI (I2C) EEPROM
This example application shows how to use the FLEXCOM module in TWI mode.
Description
This application configures the FLEXCOM peripheral in TWI mode to read and write data from an external EEPROM memory chip. Data is written to the EEPROM and then read back and compared. Successful comparison is indicated by turning on an LED.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/flexcom/twi/master/flexcom_twi_eeprom.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a7d65_curiosity.X | MPLABX project for SAMA7D65 Curiosity Board |
| sam_a7d65_curiosity_pro.X | MPLABX project for SAMA7D65 Curiosity Pro Board |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a7d65_curiosity.X | SAMA7D65 Curiosity Board |
| sam_a7d65_curiosity_pro.X | SAMA7D65 Curiosity Pro Board |
Setting Up SAMA7D65 Curiosity Board
- Connect the USBA port J3 on the board to the computer using a Type-C USB cable (to power the board)
- Connect EEPROM Click 3 Board to mikroBUS1 connector on board
Setting Up SAMA7D65 Curiosity Pro Board
- Connect the USBA port J1 on the board to the computer using a Type-C USB cable (to power the board)
- Connect EEPROM Click 3 Board to mikroBUS1 connector on board
Running the Application
- Build and run application using its IDE.
- LED indicates the success or failure:
Board LED Name SAMA7D65 Curiosity Board RGB_LED (Lights up in green color on success) SAMA7D65 Curiosity Pro Board RGB_LED (Lights up in green color on success)