1.1 ACC Interrupt
This example application shows how to use an analog comparator controller (ACC) generate an interrupt on a compare event.
Description
This example application shows how to use the ACC Peripheral library to generate an interrupt when a rising/falling edge is detected on one the analog input pins.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/acc/acc_interrupt/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a7d65_curiosity.X | MPLABX project for SAMA7D65 Curiosity Board |
| sam_a7d65_curiosity_pro.X | MPLABX project for SAMA7D65 Curiosity Pro Board |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a7d65_curiosity.X | SAMA7D65 Curiosity Board |
| sam_a7d65_curiosity_pro.X | SAMA7D65 Curiosity Pro Board |
Setting Up SAMA7D65 Curiosity Board
- Connect the USBA port J3 on the board to the computer using a Type-C® USB cable (to power the board)
- Use a jumper wire to connect Pin 40 of RPi connector to 3.3V/GND
Setting Up SAMA7D65 Curiosity Pro Board
- Connect the USBA port J1 on the board to the computer using a Type-C USB cable (to power the board)
- Use a jumper wire to connect Pin 40 of RPi connector to 3.3V/GND
Running the Application
- Build and run the application using its IDE.
- Observe LED turning on/off by
creating rising/falling edge on Pin 40 of RPi connector.
Board LED Name SAMA7D65 Curiosity Board RGB LED (Green) SAMA7D65 Curiosity Pro Board RGB LED (Green)