1.27 SHDWC Wakeup

This example application shows how to shutdown and wakeup the device using SHDWC peripheral.

Description

Application starts by toggling the LED, indicating that the device is up and running. Upon pressing the switch, it goes to Shutdown mode (stops toggling the LED). Device wakes up after 5 seconds upon RTC alarm and the LED starts toggling again.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/shdwc/rtc_wakeup.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_a7d65_curiosity.XMPLABX project for SAMA7D65 Curiosity Board
sam_a7d65_curiosity_pro.XMPLABX project for SAMA7D65 Curiosity Pro Board

Setting Up AT91Bootstrap Loader

To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_a7d65_curiosity.XSAMA7D65 Curiosity Board
sam_a7d65_curiosity_pro.XSAMA7D65 Curiosity Pro Board

Setting Up SAMA7D65 Curiosity Board

Additional hardware required:
  • SD card with FAT32 file system
Setting up the SD card:
  • Download harmony MPU bootstrap loader
  • Copy the downloaded boot loader binary( boot.bin) onto the SD card
Setting up the board:
  • SDMMC slot used for bootloading the application is SDMMC1 (J10)
  • Connect the USBA port J3 on the board to the computer using a Type-C USB cable (to power the board)
  • Connect the UART Debug port (J35) on the board to the computer using a FTDI-USB cable
  • Insert 3V CR1220 battery in BT1 battery holder

Setting Up SAMA7D65 Curiosity Pro Board

Additional hardware required:
  • SD card with FAT32 file system
Setting up the SD card:
  • Download harmony MPU bootstrap loader
  • Copy the downloaded boot loader binary( boot.bin) onto the SD card
Setting up the board:
  • SDMMC slot used for bootloading the application is SDMMC1 (J42)
  • Connect the USBA port J1 on the board to the computer using a Type-C USB cable (to power the board)
  • Connect the UART Debug port (J63) on the board to the computer using a FTDI-USB cable
  • Insert 3V CR1220 battery in BT1 battery holder

Running the Application

  1. Build the application using its IDE.
  2. Copy the output binary (named harmony.bin) onto the SD Card (Refer to the Setting up hardware section above for setting up the SD card).
  3. Insert the SD card into SDMMC slot on the board.
  4. Reset the board to run the application.
  5. LED toggles indicating the board is up and running.
  6. Press Switch A to shutdown the device (LED toggling stops).
  7. Device wakes up after 5 seconds upon RTC alarm (indicated by the LED starting to toggle again).

Following table provides details of switches and LED:

BoardSwitch ALED Name
SAMA7D65 Curiosity BoardSW2RGB_LED (Green)
SAMA7D65 Curiosity Pro BoardSW2RGB_LED (Green)